Clock frequency accuracy measurement circuit (CAC)
Below is a list of API functions output by the Code Generator for clock frequency accuracy measurement circuit use.
Table 3.4 API Functions: [Clock Frequency Accuracy Measurement Circuit]
|
API Function Name |
Function |
|
Performs initialization necessary to control the clock frequency accuracy measurement circuit. | |
|
Performs user-defined initialization relating to the clock frequency accuracy measurement circuit. | |
|
Performs processing in response to the measurement end interrupt. | |
|
Performs processing in response to the frequency error interrupt. | |
|
Performs processing in response to the overflow interrupt. | |
|
Starts measurement of the accuracy of the clock frequency. | |
|
Ends measurement of the accuracy of the clock frequency. |