Everything

Port output enable 2 (POE2)

Below is a list of API functions output by the Code Generator for port output enable 2 use.

 

Table 3.14 API Functions: [Port Output Enable 2]

API Function Name

Function

R_POE2_Create

Performs initialization necessary to control the port output enable 2.

R_POE2_Create_UserInit

Performs user-defined initialization relating to the port output enable 2.

r_poe2_oein_interrupt

Performs processing in response to the output enable interrupt n (OEIn).

R_POE2_Start

Places the MTU's complementary PWM output pins in the high-impedance state.

R_POE2_Stop

Releases the R_POE2_Stop MTU's complementary PWM output pins from the high-impedance state.

R_POE2_Set_HiZ_MTUn

Sets the high-impedance state for the MTUn pins.

R_POE2_Clear_HiZ_MTUn

Clear the high-impedance state for the MTUn pins