Event link controller (ELC)
Below is a list of API functions output by the Code Generator for event link controller use.
Table 3.10 API Functions: [Event Link Controller]
|
API Function Name |
Function |
|
Performs initialization necessary to control the event link controller. | |
|
Performs user-defined initialization relating to the event link controller. | |
|
Performs processing in response to the event link interrupt. | |
|
Starts interlinked operation of peripheral functions. | |
|
Ends interlinked operation of peripheral functions. | |
|
Generates the software event. | |
|
Sets the value of a port buffer. | |
|
Gets the value of a port buffer. |