Compare match timer W (CMTW)
Below is a list of API functions output by the Code Generator for compare match timer W use.
Table 3.21 API Functions: [Compare Match Timer W]
API Function Name |
Function |
Performs initialization necessary to control the compare match timer W. | |
Starts counting by a 16-bit timer. | |
Ends counting by a 16-bit timer. | |
Performs user-defined initialization relating to the compare match timer W. | |
Performs processing in response to the compare match interrupt. | |
Performs processing in response to the input capture interrupt. | |
Performs processing in response to the output compare interrupt. |