Performs processing in response to detection of IICA master communication error.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_iican_callback_master_error ( MD_STATUS flag );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | MD_STATUS flag; | Cause of communication error MD_SPT: Stop condition detected MD_NACK: Acknowledge not detected (No slave that matches the address/A slave can receive no more data or does not require the next data) | 
[Return value]
None.