Performs processing in response to detection of IICA slave communication error.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_iican_callback_slave_error ( MD_STATUS flag );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | MD_STATUS flag; | Cause of communication error MD_ERROR: Address mismatch detected MD_NACK: Acknowledge not detected (Master receiving end) | 
[Return value]
None.