Starts IICA slave transmission.
Remark This API function repeats the byte-level IICA slave transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
[Syntax]
#include “r_cg_macrodriver.h”
void R_IICAn_Slave_Send ( uint8_t * const tx_buf, uint16_t tx_num );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | uint8_t * const tx_buf; | Pointer to a buffer storing the transmission data | 
| I | uint16_t tx_num; | Total amount of data to send | 
[Return value]
None.