Starts IICA master reception.
Remark This API function performs byte-level IICA master reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include “r_cg_macrodriver.h”
MD_STATUD   
R_IICAn_Master_Receive ( uint8_t adr, uint8_t * const 
rx_buf,
 uint16_t rx_num, uint8_t wait 
);
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | uint8_t adr; | Slave address | 
| O | uint8_t * const rx_buf; | Pointer to a buffer to store the received data | 
| I | uint16_t rx_num; | Total amount of data to receive | 
| I | uint8_t wait | Setup time of start conditions | 
[Return value]
| Macro | Description | 
| MD_OK | Normal completion | 
| MD_ERROR1 | Bus communication status | 
| MD_ERROR2 | Bus not released status |