Starts IICA slave reception.
Remark This API function performs byte-level IICA slave reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include “r_cg_macrodriver.h”
void R_IICAn_Slave_Receive ( uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| O | uint8_t * const rx_buf; | Pointer to a buffer to store the received data | 
| I | uint16_t rx_num; | Total amount of data to receive | 
[Return value]
None.