long double __far acosl(long double x); (C99)
Returns the arc cosine of x. The returned value is in radian and in a range of [0, π].
If x is not between [-1, 1], acosl returns a Not-a-Number (NaN) and sets macro EDOM to global variable errno.
This function calculates the arc cosine of x. Specify x as, -1<= x <= 1.