Returns the arc tangent (arctangent) of x. The returned value is in radian and in a range of [-π / 2, π / 2].
When x is Not-a-Number, this function returns Not-a-Number and sets macro EDOM to global variable errno.
When x is -0, this function returns -0.
If the solution is a denormal number, atan sets macro ERANGE to global variable errno.