long double __far tanl(long double x); (C99)
If x is Not-a-Number or ±∞, tanl returns a Not-a-Number (NaN) and sets macro EDOM to global variable errno.
If the solution is a denormal number, tanl sets macro ERANGE to global variable errno.
This function calculates the cosine of x. Specify the angle in radian.