Calculates the absolute value
[Classification]
Mathematical library
[Syntax]
#include <math.h>
float __far fabsf(float x);
[Return value]
Returns the absolute value (size) of x.
If x is ±∞, fabsf returns ±∞ and sets macro ERANGE to global variable errno.
If x is a Not-a-Number(NaN), fabsf returns a Not-a-Number (NaN) and sets macro EDOM to global variable errno.
[Description]
This function calculates the absolute value (size) of x.