Divide floating-point number into integer and decimal
float __far modff(float val, float *iptr);
Returns a signed decimal part. The sign of the result is the same as the sign of val.
When val is ±∞, this function returns 0 and sets ±∞ to iptr and macro EDOM to global variable errno.
When val is Not-a-Number, this function returns Not-a-Number and sets Not-a-Number to iptr and macro EDOM to global variable errno.
This function divides val into integer and decimal parts, and stores the integer part in *iptr. The sign of the integer and decimal parts is the same as the sign of val.