Everything

pow


Calculates the yth power of x.

[Classification]

Mathematical library

[Syntax]

#include <math.h>

double __far pow(double x, double y);

[Return value]

Returns the yth power of x.

If x < 0 and y is a non-integer or if x = 0 and y <= 0, pow returns a Not-a-Number (NaN) and sets the macro EDOM for the global variable errno.

If an overflow occurs, pow returns ±∞ and sets the macro ERANGE for errno.

If an underflow occurs, pow returns a denormal number and sets the macro ERANGE for errno.

[Description]

This function calculates the yth power of x.