Everything
 

Select Pseudo-Error dialog box [Full-spec emulator][E1][E20]


This dialog box is used to select ECM pseudo-errors displayed in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].

Figure A.58

Select Pseudo-Error Dialog Box

 

This section describes the following.

[How to open]

-

On the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20], click the [Select Pseudo-Error...] button on the toolbar.

[Description of each area]

(1)

[ECM Pseudo-error List]

A list of pseudo-errors managed by the ECM is displayed.

When a check box is selected, the pseudo-error is regarded as a target in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].

(2)

Button area

Select All Pseudo-Error

Selects check boxes of all pseudo-errors in [ECM Pseudo-Error List].

Clear All Pseudo-Error

Clears check boxes of all pseudo-errors in [ECM Pseudo-Error List].

[Function buttons]

Button

Function

OK

Registers the pseudo-errors that were selected in this dialog box to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20] and deletes the unselected pseudo-errors from the panel.

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.