This dialog box is used to display and modify detailed information on an execution-related event selected in the Events panel.


This section describes the following.
On the Events panel, move the caret to any one of the following events, and then select [Edit Condition...] from the context menu. |
Execution-related event as start and end condition in detailed information on Performance Measurement event |
Specify the address condition.
Specify the condition to compare address. The condition for an access event being generated varies with the value of this setting. [Inside the range (<=Addresses<=)] / [Outside the range !(<=Addresses<=)] |
||||
Specifies the address with [Address]. |
||||
Specifies the range with [Start address] and [End address]. |
||||
This item appears only when [Specified address (==)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition]. |
||||
This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition]. |
||||
This item appears only when [Inside the range (<=Addresses<=)] or [Outside the range !(<=Addresses<=)] is selected in [Compare condition]. |
||||
Specify whether to specify an address mask. This item appears only when [Specified address (==)] is selected in [Compare condition]. |
||||
Specify the value of address mask. This item appears only when [Use the address mask] is set to [Yes]. |
||||
Specify the pass count condition.
The relevant event occurs when the event condition is met as many times as the specified pass count. |
||||
This area displays a simple description of the item selected in the Event conditions setting area.
Displays all categories in the Event conditions setting area. |
||
Hides categories in the Event conditions setting area and rearranges only setting items in the ascending order |
||