16-bit timer pulse unit (TPU)
Below is a list of API functions output by the Code Generator for 16-bit timer pulse unit use.
Table 3.17 API Functions: [16-bit timer pulse unit]
API Function Name |
Function |
Performs initialization necessary to control the 16-bit timer pulse unit. | |
Starts counting by a 16-bit timer. | |
Ends counting by a 16-bit timer. | |
Performs user-defined initialization relating to the 16-bit timer pulse unit. | |
Performs processing in response to the input capture/compare match interrupt. | |
Performs processing in response to the overflow interrupt. | |
Performs processing in response to the underflow interrupt. |