Buses
Below is a list of API functions output by the Code Generator for buses use.
Table 3.7 API Functions: [Buses]
API Function Name |
Function |
Performs initialization necessary to control the buses. | |
Performs user-defined initialization relating to the buses. | |
Performs processing in response to the bus error (illegal address access). | |
Allows the detection of bus errors (illegal address access). | |
Prohibits the detection of bus errors (illegal address access). | |
Performs initialization of SDRAM controller. |