FIFO embedded serial communications interface (SCIFA)
Below is a list of API functions output by the Code Generator for FIFO embedded serial communications interface use.
Table 3.26 API Functions: [FIFO Embedded Serial Communications Interface]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the FIFO embedded serial communications interface.  | |
| 
       Starts FIFO embedded SCI communication.  | |
| 
       Ends FIFO embedded SCI communication.  | |
| 
       EStarts FIFO embedded SCI transmission (asynchronous mode).  | |
| 
       Starts FIFO embedded SCI reception (asynchronous mode).  | |
| 
       Starts FIFO embedded SCI transmission/reception (clock synchronous mode).  | |
| 
       Performs user-defined initialization relating to the FIFO embedded serial communications interface.  | |
| 
       Performs processing in response to the transmit-end interrupts.  | |
| 
       Performs processing in response to the transmit FIFO data empty interrupts.  | |
| 
       Performs processing in response to the receive FIFO data full interrupts.  | |
| 
       Performs processing in response to the framing error or parity error interrupts.  | |
| 
       Performs processing in response to the break or overrun interrupts.  | |
| 
       Performs processing in response to the receive data ready interrupts.  | |
| 
       Performs processing in response to the transmit-end interrupts.  | |
| 
       Performs processing in response to the receive FIFO data full interrupts.  | |
| 
       Performs processing in response to the error interrupts.  |