8-bit timer (TMR)
Below is a list of API functions output by the Code Generator for 8-bit timer use.
Table 3.18 8 API Functions: [8-bit timer]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 8-bit timer pulse unit.  | |
| 
       Starts counting by an 8-bit timer.  | |
| 
       Ends counting by an 8-bit timer.  | |
| 
       Performs user-defined initialization relating to the 8-bit timer pulse unit.  | |
| 
       Performs processing in response to the compare match interrupt.  | |
| 
       Performs processing in response to the overflow interrupt.  |