本API関数では,データ(引数adrで指定されたスレーブ・アドレスとR/W#ビット)をスレーブ・デバイスにSCIマスタ送信したのち,引数tx_bufで指定されたバッファから1バイト単位のSCIマスタ送信を引数tx_numで指定された回数だけ繰り返し行います。 |
本API関数では,SCIマスタ送信の開始処理として,内部的にR_SCIn_IIC_StartConditionの呼び出しを行っています。 |
SCIマスタ送信を行う際には,本API関数の呼び出し以前にR_SCIn_Startを呼び出す必要があります。 |
#include "r_cg_macrodriver.h" void R_SCIn_IIC_Master_Send ( uint8_t adr, uint8_t * const tx_buf, uint16_t tx_num ); |