|
r_atuiv_timerknm_callback_cycle
|
Performs processing in response to the cycle match interrupt.
Remark | This API function is called as the callback routine of interrupt process r_atuiv_timerknm_interrupt corresponding to the cycle match interrupt. |
Syntax
void r_atuiv_timernm_channelm_cycle_callback ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
Argument(s)
None.
Return value
None.