Renesas Electronics
R_ATUIV_Timerkn_Create_UserInit
Performs user-defined initialization relating to the each timer functions.
Remark
This API functions is called as the R_ATUIV_Timerkn_Create callback routine.
Syntax
void R_ATUIV_Timerk_Create_UserInit ( void );
void R_ATUIV_Timerkn_Create_UserInit ( void );
k is the timer kind, n is the unit number.
Argument(s)
None.
Return value