R_ATUIV_Timerknm_Set_Compare_Match


Sets the compare match register.

Syntax

void    R_ATUIV_Timerknm_Set_Compare_Match ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

Argument(s)

None.

Return value

None.