Renesas Electronics
r_atuiv_timerknm_callback_duty
Performs processing in response to the duty match interrupt.
Remark
This API function is called as the callback routine of interrupt process r_atuiv_timerknm_interrupt corresponding to the duty match interrupt.
Syntax
void r_atuiv_timerknm_callback_duty ( void );
k is the timer kind, n is the unit number, m is the channel number.
Argument(s)
None.
Return value