R_ATUIV_Timerknm_Start_Down_Count


Starts the down count.

Syntax

void    R_ATUIV_Timerknm_Start_Down_Count ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

Argument(s)

None.

Return value

None.