| 
 R_ATUIV_Timerknm_xpin_Output_Low 
 | 
Output of pin provides low output.
Syntax
void    R_ATUIV_Timerknm_xpin_Output_Low ( void ); 
 | 
 
Remark  | k is the timer kind, n is the unit number, m is the channel number, x is the output pin.  | 
 
Argument(s)
None.
Return value
None.