|
r_atuiv_timerknm_overflow_interrupt
|
Performs processing in response to the overflow interrupt.
Syntax
void r_atuiv_timerknm_overflow_interrupt ( void );
|
void r_atuiv_timerknm_overflow1_interrupt ( void );
void r_atuiv_timerknm_overflow2_interrupt ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
Argument(s)
None.
Return value
None.