Halts the clock supplied to the serial array unit.
Remark | Calling this API function changes the serial array unit to reset status.
For this reason, writes to the control registers (e.g. serial clock select register n: SPSn) after this API function is called are ignored.
|
[Syntax]
void R_SAUm_Set_PowerOff ( void );
|
Remark | m is the unit number. |
[Argument(s)]
None.
[Return value]
None.