|
|
R_SAUm_Create
|
Performs initialization necessary to control the serial array unit.
|
R_SAUm_Create_UserInit
|
Performs user-defined initialization related to the serial array unit.
|
R_SAUm_Reset
|
Reset the serial array unit.
|
R_SAUm_Set_PowerOff
|
Halts the clock supplied to the serial array unit.
|
R_SAUm_Set_SnoozeOn
|
Enables the switch from STOP mode to SNOOZE mode.
|
R_SAUm_Set_SnoozeOff
|
Disables the switch from STOP mode to SNOOZE mode.
|
R_UARTn_Create
|
Performs initialization necessary to perform the UART communication.
|
r_uartn_interrupt_send
|
Performs processing in response to the UART transmission end interrupt INTSTn.
|
r_uartn_interrupt_receive
|
Performs processing in response to the UART reception end interrupt INTSRn.
|
r_uartn_interrupt_error
|
Performs processing in response to the reception error interrupt INTSREn.
|
R_UARTn_Start
|
Sets UART communication to standby mode.
|
R_UARTn_Stop
|
Ends UART communication.
|
R_UARTn_Send
|
Starts UART data transmission.
|
R_UARTn_Receive
|
Starts UART data reception.
|
r_uartn_callback_sendend
|
Performs processing in response to the UART transmission end interrupt INTSTn.
|
r_uartn_callback_receiveend
|
Performs processing in response to the UART reception end interrupt INTSRn.
|
r_uartn_callback_error
|
Performs processing in response to the UART reception error interrupt INTSREn.
|
r_uartn_callback_softwareoverrun
|
Performs processing in response to detection of overrun error.
|
R_CSImn_Create
|
Performs initialization necessary to perform the 3-wire serial I/O communication.
|
r_csimn_interrupt
|
Performs processing in response to the CSI communication end interrupt INTCSImn.
|
R_CSImn_Start
|
Sets 3-wire serial I/O communication to standby mode.
|
R_CSImn_Stop
|
Ends 3-wire serial I/O communication.
|
R_CSImn_Send
|
Starts CSI data transmission.
|
R_CSImn_Receive
|
Starts CSI data reception.
|
R_CSImn_Send_Receive
|
Starts CSI data transmission/reception.
|
r_csimn_callback_sendend
|
Performs processing in response to the CSI transmission end interrupt INTCSImn.
|
r_csimn_callback_receiveend
|
Performs processing in response to the CSI reception end interrupt INTCSImn.
|
r_csimn_callback_error
|
Performs processing in response to the CSI reception error interrupt INTSREn.
|
R_IICmn_Create
|
Performs initialization necessary to perform the simplified IIC communication.
|
r_iicmn_interrupt
|
Performs processing in response to the simple IIC communication end interrupt INTIICmn.
|
R_IICmn_StartCondition
|
Generates start conditions.
|
R_IICmn_StopCondition
|
Generates stop conditions.
|
R_IICmn_Stop
|
Ends simplified IIC communication.
|
R_IICmn_Master_Send
|
Starts simple IIC master transmission.
|
R_IICmn_Master_Receive
|
Starts simple IIC master reception.
|
r_iicmn_callback_master_sendend
|
Performs processing in response to the simple IICmn master transmission end interrupt INTIICmn.
|
r_iicmn_callback_master_receiveend
|
Performs processing in response to the simple IICmn master reception end interrupt INTIICmn.
|
r_iicmn_callback_master_error
|
Performs processing in response to detection of parity error (ACK error).
|