Performs processing in response to the simple IICmn master reception end interrupt INTIICmn.
This API function is called as the callback routine of interrupt process r_iicmn_interrupt corresponding to the simple IICmn master reception end interrupt INTIICmn (performed when number of received data specified by R_IICmn_Master_Receive argument rx_num has been completed). |