Performs processing in response to the CSI transmission end interrupt INTCSImn.
This API function is called as the callback routine of interrupt process r_csimn_interrupt corresponding to the CSI transmission end interrupt INTCSImn (performed when number of transmission data specified by R_CSImn_Send or R_CSImn_Send_Receive argument tx_num has been completed). |