This API function is used as an internal function of R_IICmn_Master_Send and R_IICmn_Master_Receive.
For this reason, there is normally no need to call it from a user program.
[Syntax]
void R_IICmn_StartCondition ( void );
Remark
m is the unit number, and n is the channel number.