Performs processing in response to the CSI communication end interrupt INTCSImn.
Remark | This API function is called as the interrupt process corresponding to the CSI communication end interrupt INTCSImn. |
[Syntax]
__interrupt static void r_csimn_interrupt ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.