Performs initialization necessary to perform the simplified IIC communication.
Remark | This API function is used as an internal function of R_SAUm_Create.
For this reason, there is normally no need to call it from a user program.
|
[Syntax]
void R_IICmn_Create ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.