RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20]


This dialog box is used to make settings related to the entire RS-CAN module shown in the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].

Figure A.61

RS-CAN Module Setting Dialog Box

 

This section describes the following.

[How to open]

-

On the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20], click the [RS-CAN Module Setting...] button on the toolbar.

[Description of each area]

(1)

RS-CAN setting area

Set up the entire RS-CAN.

(a)

[CAN bus clock source]

Select the clock source for the RS-CAN module from the following drop-down list.

Value

Meaning

clk_xincan

Clock supplied to clk_xincan of RS-CAN

clkc

Clock supplied to clkc of RS-CAN

The actual frequency of the specified clock source appears at the bottom of the drop-down list.

(b)

[Use timestamp function]

Specify whether the timestamp function of the RS-CAN is to be used.

(c)

[Use DLC check function]

Specify whether the Data Length Code (DLC) checking function of the RS-CAN is to be used.

(d)

[Use DLC replacement function]

Specify whether the DLC replacement function of the RS-CAN is to be used.

This item is specifiable only when the DLC checking function is used.

[Function buttons]

Button

Function

OK

Reflects the clock source, timestamp, DLC checking function, and DLC replacement function settings that were made in this dialog box to the [RS-CAN settings] area on the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.