Renesas Electronics
Below is a list of API functions output by the Code Generator for buses use.
Table 3.7
API Functions: [Buses]
API Function Name
Function
R_BSC_Create
Performs initialization necessary to control the buses.
R_BSC_Create_UserInit
Performs user-defined initialization relating to the buses.
r_bsc_buserr_interrupt
Performs processing in response to the bus error (illegal address access).
R_BSC_Error_Monitoring_Start
Allows the detection of bus errors (illegal address access).
R_BSC_Error_Monitoring_Stop
Prohibits the detection of bus errors (illegal address access).
R_BSC_InitializeSDRAM
Performs initialization of SDRAM controller.