Renesas Electronics
Below is a list of API functions output by the Code Generator for serial peripheral interface use.
Table 3.28
API Functions: [Serial Peripheral Interface]
API Function Name
Function
R_RSPIn_Create
Performs initialization necessary to control the serial peripheral interface.
R_RSPIn_Create_UserInit
Performs user-defined initialization relating to the serial peripheral interface.
r_rspin_receive_interrupt
Performs processing in response to the receive buffer full interrupts.
r_rspin_transmit_interrupt
Performs processing in response to the transmit buffer error interrupts.
r_rspin_error_interrupt
Performs processing in response to the RSPI error interrupts.
r_rspin_idle_interrupt
Performs processing in response to the RSPI idle interrupts.
R_RSPIn_Start
Starts RSPI communication.
R_RSPIn_Stop
Ends RSPI communication.
R_RSPIn_Send
Starts RSPI transmission.
R_RSPIn_Send_Receive
Starts RSPI transmission/reception.
r_rspin_callback_receiveend
r_rspin_callback_error
r_rspin_callback_transmitend