Renesas Electronics
Below is a list of API functions output by the Code Generator for 16-bit timer pulse unit use.
Table 3.17
API Functions: [16-bit timer pulse unit]
API Function Name
Function
R_TPU_Create
Performs initialization necessary to control the 16-bit timer pulse unit.
R_TPU_Create_UserInit
Performs user-defined initialization relating to the 16-bit timer pulse unit.
r_tpu_tginm_interrupt
Performs processing in response to the input capture/compare match interrupt.
r_tpu_tcinv_interrupt
Performs processing in response to the overflow interrupt.
r_tpu_tcinu_interrupt
Performs processing in response to the underflow interrupt.
R_TPUn_Start
Starts counting by a 16-bit timer.
R_TPUn_Stop
Ends counting by a 16-bit timer.