Renesas Electronics
Below is a list of API functions output by the Code Generator for 12-bit D/A converter use.
Table 3.32
API Functions: [12-Bit D/A Converter]
API Function Name
Function
R_R12DA_Create
Performs initialization necessary to control the 12-bit D/A converter.
R_DA_Create_UserInit
Performs user-defined initialization relating to the 12-bit D/A converter.
R_R12DAn_Start
Starts D/A conversion.
R_R12DAn_Stop
Ends D/A conversion.
Starts synchronous D/A conversion.
Ends synchronous D/A conversion.
R_R12DAn_Set_ConversionValue
Sets the data for D/A conversion.