3.2.14  
Port output enable 2 (POE2)
 
Below is a list of API functions output by the Code Generator for port output enable 2 use.
| 
Table 3.14 | API Functions: [Port Output Enable 2] | 
|  |  | 
| 
R_POE2_Create | 
Performs initialization necessary to control the port output enable 2. | 
| 
R_POE2_Create_UserInit | 
Performs user-defined initialization relating to the port output enable 2. | 
| 
r_poe2_oein_interrupt | 
Performs processing in response to the output enable interrupt n (OEIn). | 
| 
R_POE2_Start | 
Places the MTU's complementary PWM output pins in the high-impedance state. | 
| 
R_POE2_Stop | 
Releases the R_POE2_Stop MTU's complementary PWM output pins from the high-impedance state. | 
| 
R_POE2_Set_HiZ_MTUn | 
Sets the high-impedance state for the MTUn pins. | 
| 
R_POE2_Clear_HiZ_MTUn | 
Clear the high-impedance state for the MTUn pins |