Renesas Electronics
Below is a list of API functions output by the Code Generator for clock generation circuit use.
Table 3.2
API Functions: [Clock Generation Circuit]
API Function Name
Function
R_CGC_Create
Performs initialization required to control the clock generation circuit.
R_CGC_Create_UserInit
Performs user-defined initialization relating to the clock generation circuit.
r_cgc_oscillation_stop_interrupt
Performs processing in response to the osillation stop detection interrupt.
r_cgc_oscillation_stop_nmi_interrupt
Performs processing in response to the oscillation stop detection NMI.
R_CGC_Set_ClockMode
Sets the clock source.