Performs processing in response to detection of IICA master communication error.
[Syntax]
#include r_cg_macrodriver.h
static void r_iican_callback_master_error ( MD_STATUS flag );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
I |
MD_STATUS flag; |
Cause of communication error MD_SPT: Stop condition detected MD_NACK: Acknowledge not detected (No slave that matches the address/A slave can receive no more data or does not require the next data) |
[Return value]
None.