R_IICAn_Set_PowerOff

Halts the clock supplied to the serial interface IICA.

Remark Calling this API function changes the serial interface IICA to reset status.
For this reason, writes to the control registers (e.g. IICA control register n: IICCTLn) after this API function is called are ignored.

[Syntax]

void R_IICAn_Set_PowerOff ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.