Performs processing in response to detection of IICA slave communication error.
[Syntax]
#include r_cg_macrodriver.h
static void r_iican_callback_slave_error ( MD_STATUS flag );
Remark n is the channel number.
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 I  | 
 MD_STATUS flag;  | 
 Cause of communication error MD_ERROR: Address mismatch detected MD_NACK: Acknowledge not detected (Master receiving end)  | 
[Return value]
None.