r_iican_callback_slave_sendend

Performs processing in response to the IICA slave transmission end interrupt INTIICAn.

Remark This API function is called as the callback routine of interrupt process r_iican_interrupt corresponding to the IICA slave transmission end interrupt INTIICAn.

[Syntax]

static void r_iican_callback_master_sendend ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.