Starts IICA slave reception.
Remark This API function performs byte-level IICA slave reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include r_cg_macrodriver.h
void R_IICAn_Slave_Receive ( uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
O |
uint8_t * const rx_buf; |
Pointer to a buffer to store the received data |
I |
uint16_t rx_num; |
Total amount of data to receive |
[Return value]
None.