Receive 4Bytes data by Slave.
[GUI setting example]
| 
 Serial  | 
 Used  | |||
| 
 SAU0  | 
 Unused  | |||
| 
 SAU1  | 
 Unused  | |||
| 
 IICA0  | 
 Used  | |||
| 
 Transfer mode  | 
 Slave  | |||
| 
 Slave0  | 
||||
| 
 Clock mode setting  | 
 fCLK/2  | |||
| 
 Local address setting  | 
 0xA0  | |||
| 
 Operation mode setting  | 
 Normal  | |||
| 
 Wakeup function setting  | 
 Off  | |||
| 
 Communication endinterrupt priority (INTIICA0)  | 
 Low  | |||
| 
 Slave transmission end (Callback function setting)  | 
 Unused  | |||
| 
 Slave reception end (Callback function setting)  | 
 Used  | |||
| 
 Slave error (Callback function setting)  | 
 Unused  | |||
[API setting example]
r_main.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_iica0_rx_buf[4];
/* End user code. Do not edit comment generated here */
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Receive data as slave mode */
R_IICA0_Slave_Receive((uint8_t *)g_iica0_rx_buf, 4U);
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_serial_user.c
static void r_iica0_callback_slave_receiveend(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop IICA0 module operation */
R_IICA0_Stop();
/* End user code. Do not edit comment generated here */
}