Starts IICA master reception.
Remark This API function performs byte-level IICA master reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include r_cg_macrodriver.h
MD_STATUD 
R_IICAn_Master_Receive ( uint8_t adr, uint8_t * const 
rx_buf,
uint16_t rx_num, uint8_t wait 
);
Remark n is the channel number.
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 I  | 
 uint8_t adr;  | 
 Slave address  | 
| 
 O  | 
 uint8_t * const rx_buf;  | 
 Pointer to a buffer to store the received data  | 
| 
 I  | 
 uint16_t rx_num;  | 
 Total amount of data to receive  | 
| 
 I  | 
 uint8_t wait  | 
 Setup time of start conditions  | 
[Return value]
| 
 Macro  | 
 Description  | 
| 
 MD_OK  | 
 Normal completion  | 
| 
 MD_ERROR1  | 
 Bus communication status  | 
| 
 MD_ERROR2  | 
 Bus not released status  |